Loading
Blog
Recent ActivityRecent Activity

Two Low-Cost Technologies are Transforming Plant Floors

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Plex_Blog_151207_TwoLow

Manufacturing facilities are filled with expensive equipment. Multi-million-dollar investments can make, or break, a company’s ability to compete and grow. But in today’s connected shop floor environment, smaller, low-cost tools are delivering competitive advantage.

Today, sensors and smart tools are helping manufacturers produce higher-quality products at a lower cost. Let’s take a look at the impact these devices are already having.

Materials and Components in Constant View

While some manufacturers still leverage whiteboards and tracking sheets for inventory, modern manufacturers now use sensors in the form of low-power Bluetooth, smart tags, and even RFID tags to maintain visibility of any item that remains in constant motion during manufacturing.

Consider the journey of raw materials that begins at a supplier site. Material is transported via truck, ship, etc. to a manufacturing plant. From there, it is transformed into a final product. Along the way sensors, tags and smart labels, coupled with ubiquitous wireless and cellular networks, allow manufacturers to monitor and trace both the materials and their path to product.

Not only can these sensors track location, they can report data about the temperature and turbulence materials endure en route. The cost of these new technologies today can be anything from a few dollars down to a few cents, putting experimentation and trials on the shop floor well into reach for most operations.

Cloud ERP systems are a huge catalyst for data collection and sharing of complex manufacturing, design, and costing information. Unlike legacy systems, adding the connectivity required to grab data from new sensors and tags doesn’t require new development or a new hardware stack.

Smart Tools Take Human Error Out of the Equation

Smart tools that connect to a cloud ERP system are a key aspect of the ongoing cycle of innovation and cost reduction because they make highly complex production lines possible. The torque wrench is a perfect example. For more than 100 years, the torque wrench has been an essential tool for manufacturers because it applies specific torque to a fastener, such as a nut or bolt. The ability to apply a specific amount of torque can make the difference in the performance of an end product.

Today, connected torque wrenches can automatically adjust based on individual product specifications, accelerating the speed of production, improving the accuracy of execution and traceability. For a torque wrench in the assembly of a complex part:

  • The cloud ERP system captures the torque applied to each part, the specific wrench that was used, when that wrench was last calibrated, and the employee who used it.
  • In each future assembly, the cloud system will identify the specifications for each part and instruct the wrench to automatically apply the correct level of torque. This means that mistakes can be essentially eliminated, even on a dynamic production line. 
  • If a company later learns that the wrench was faulty in some way, the ERP system, using information gathered and organized in the cloud, can identify every part affected. Any product recall can be speedy and precisely focused on the right products.

The IP torque wrench is one example of how manufacturers can improve operations as they increase the connections between people, tools, and products on the plant floor. Like sensors, up-front costs are going down dramatically. At the same time, connectivity inherent in new Cloud ERP solutions makes adding smart tools to a connected manufacturing environment simple. Instead of traditional design/development processes involving extensive custom code and bespoke systems, tools like IP wrenches and quality testing gear can be added to shop floor operations in minutes. Looking ahead, it may not be the most expensive tool in the shop that has the biggest impact.

Topics: Aerospace Automotive High Tech & Electronics Industrial Manufacturing Plastics & Rubber Precision Metalforming

Plex Team
Plex Team
Plex, by Rockwell Automation, is the leader in cloud-delivered smart manufacturing solutions, empowering the world’s manufacturers to make awesome products. Our platform gives manufacturers the ability to connect, automate, track and analyze every aspect of their business to drive transformation. The Plex Smart Manufacturing Platform includes solutions for manufacturing execution (MES), ERP, quality, supply chain planning and management, Industrial IoT and analytics to connect people, systems, machines, and supply chains, enabling them to lead with precision, efficiency and agility.

Related Articles

Loading
Loading