Loading
Blog
Recent ActivityRecent Activity

MRP and Inventory Management

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail

Most companies use Material Requirement Planning (MRP) software, or an MRP module of an ERP, to plan and manage the purchase, production, and transfer orders of finished goods and components based on a demand plan or forecast. It is time-phased and can manage large numbers of materials—and bill of materials—to ensure the right components are ordered and on hand to support production-scheduling software.

Yet, MRP systems cannot do everything. Materials Managers have to ensure that data is accurate, and supply attributes are set optimally, which can be non-trivial and can make or break the effectiveness of an MRP:

  • The Bill of Materials has to be up to date. These are not static documents. Specifications change resulting in changes of suppliers, this information must be accurate.
  • The lead times for all component and supplier locations must be up to date including the transit times. Shipping times and suppliers are changing, and sometimes location change as well.
  • Forecasts and/or demand plans must be constantly updated, and every effort should be taken to make them as accurate as possible. This is critical in MTS environments and MTO scenarios because you need to ensure components and capacities are available to meet those future requirements.

All of the above data is crucial in their own right, but they also contribute to the calculations of re-order points and buffer inventories for all finished goods and materials. MRP systems generally do not calculate or evaluate re-order points and inventory buffers. In the rare occasions that they do, they might not be using the calculations best suited for your particular business.

How often should you recalculate the inventory parameters?

This depends on the growth or decay of the business in general. It also depends on the volatility of the business environments. According to ISM in the "The Next Challenge for Global Growth: Keeping Up With Demand" article published in the April 24th edition of the Wall Street Journal: Economic data are also showing a constrained supply side. The Institute for Supply Management’s index measuring backlogs of orders in manufacturing has reached its highest level since May 2004. Set against robust demand, supply chains are “struggling to keep up,” the ISM says.

Regardless, if the issue is demand or supply related, MRP systems are not suited for analyzing and resetting demand and supply attributes on a continuous basis. Most companies do these calculations and evaluations themselves in home-grown software or spreadsheets. Others use third-party software specifically designed to size and calculate the inventory parameters on a rolling basis, while populating the MRP with re-orders points and buffers over the next 6-12 months.

MRP's Bottom Line

The bottom line is that MRP systems are very good and may be the central engine for managing inventory and ensuring customer service. However, MRP systems require good data and the setting of optimal parameters to run effectively. This includes the periodic recalculation of re-order points and buffers often best done by specialty software such as Plex Supply Chain Planning.

It is interesting to also note, when we first built Plex Supply Chain Planning it was done so with the inclusion of a robust MRP engine in order to properly visualize the impact of demand and supply on both a short- and long-term basis. By better visualizing your reality, we help you move from reactive responses to more proactive decisions.

Today, many of our customers prefer to use Plex Supply Chain Planning in place of their ERP systems since it moves all the MRP-related parameters out of your ERP's black box, making it easier to modify settings and view the impact before taking action. These orders can then be pushed back to your ERP for execution.

Topics: Supply Chain Management Planning

Plex Team
Plex Team
Plex, by Rockwell Automation, is the leader in cloud-delivered smart manufacturing solutions, empowering the world’s manufacturers to make awesome products. Our platform gives manufacturers the ability to connect, automate, track and analyze every aspect of their business to drive transformation. The Plex Smart Manufacturing Platform includes solutions for manufacturing execution (MES), ERP, quality, supply chain planning and management, Industrial IoT and analytics to connect people, systems, machines, and supply chains, enabling them to lead with precision, efficiency and agility.

Related Articles

Loading
Loading