Loading
Blog
Recent ActivityRecent Activity

The Delicate Balance of Safety Stock vs. Safety Time

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail

With disruption such as COVID-19 rapidly shifting consumer tastes, market volatility, and human error, the threat of both overstock and stockouts is always present. On the one hand, companies strive to have enough stock available to manage their order position and fulfill service level agreements. On the other, excess inventory can drive up costs and restrict cash flow. So what part does safety stock or safety time play in this?

Safety Stock and Safety Time

One way to ensure order fulfillment is by using safety stock – that extra edge used as a buffer between orders and on-hand inventory that allows a company to achieve high service levels and maintain customer satisfaction. The retention of safety stock is an attempt to capture forecasted demand for a product. However, the caveat is that you understand that demand in the first place.

Safety time is an attempt to leverage lead times to ensure that materials and supplies arrive just in time for the correct production level. It may be based on actual lead time if there are few, or even a single, component and supply is predictable. Or a company may use a more complex analysis that includes considerations such as internal review, supplier lead time, transportation, and other factors.

Striking a Balance

While each method has distinct advantages and disadvantages, they are often used together. In companies with a sophisticated supply chain management system, the balance between the two can be managed efficiently. But in those whose supply chain management is still plagued by spreadsheets, disparate and siloed internal systems, and “gut feeling”, there is a danger of creating problems in their supply chain.

One such problem can arise when safety time does not capture or recognize rising demand quickly enough. If lead times from suppliers tend to run long, or if the material comes from abroad, seasonal demand or other unforeseen surges in orders can result in shortages by the time the product arrives. If the surge is large enough, safety stock levels may be depleted before arrival. In the above case, failure by the planning system to recognize or capture demand can push it into expediting mode. This impacts profitability in the form of lost sales or cancelled orders as well as adding expensive expediting costs to Cost of Goods Sold (COGS). And if the misstep is big enough, or continues to happen, it can throw the entire planning system into a spiral.

Of course, the opposite scenario is a concern as well. By missing demand signals, a company may not detect trending drops in sales due to disruption, changing consumer tastes, or other factors. In these cases, if automatic replenishment quantities – or human analytical shortcomings – continue to kick in, even as demand drops, both safety time and safety stock calculations become moot as the company begins to carry too much inventory.

The tendency of many decision-makers is almost always to err on the side of extra stock “just in case”. But when that instinct is coupled with missed demand signals, a company can find itself overwhelmed with stock. This drives up holding costs and may result in the company having to take on additional warehouse space, adding cost at a time when orders are slowing.

Considerations for Balancing Safety Stock and Safety Time

For companies looking to balance safety stock with safety time, there are a few things to consider:

  1. Set Safety Time Based on Demand – If safety time were as simple as setting reorder points based on lead times, everyone’s forecast would be 100% accurate all the time. But that doesn’t reflect the real world. Accurate demand planning can highlight the optimal safety time to result in optimal safety stock. This requires demand planning that is insightful, and data-driven.
  2. Manage Trends and Seasons – Most companies know their rough seasonal periods. But they can shift over time. The same is true for trends. Larger trends are easy to spot and account for, while micro-trends or fast movers may go undetected. By accurately capturing demand signals, planners can create a more dynamic balance for both safety time and safety stock because the demand data is the driver rather than item quantity and lead time.
  3. Identify Demand Uncertainty – If a company’s supplies are generally local, lead times may be shorter and dependable. If they are global, then transportation, customs, minimum order quantities may result in longer and more unpredictable lead times. And for complex production processes, there may be a mix of both. Identifying and analyzing which situation reflects a company’s order reality can help establish an accurate formula for setting both safety stock and safety time.

Automating Demand Planning

The most effective way to balance safety stock and safety time is with demand and supply software. Using advanced analytics, near real-time data can be combined with historical data to drive optimum economic order quantities and set both stock and lead time targets that align with demand. 

oday’s demand and supply automation software also offer tools such as “what if” scenario planning, and ABC analysis to focus stock and inventory levels on the most profitable products. Combined with time-phased inventory forecasting, tasks such as order timing and quantity can be automated with confidence.

If your company is mired down in spreadsheets, manual overrides, and miscommunication between planners and suppliers, Plex Supply Chain Planning offers Supply Chain Planning software that helps you put demand in control of supply. By automating your supply planning with Plex Supply Chain Planning, you can confidently reduce demand uncertainty to find the best balance between safety stock and safety time for your business.

Topics: Supply Chain Management Planning

Plex Team
Plex Team
Plex, by Rockwell Automation, is the leader in cloud-delivered smart manufacturing solutions, empowering the world’s manufacturers to make awesome products. Our platform gives manufacturers the ability to connect, automate, track and analyze every aspect of their business to drive transformation. The Plex Smart Manufacturing Platform includes solutions for manufacturing execution (MES), ERP, quality, supply chain planning and management, Industrial IoT and analytics to connect people, systems, machines, and supply chains, enabling them to lead with precision, efficiency and agility.

Related Articles

Loading
Loading