Loading
page_container_1 w:2160.0 h:3168.0

THE ROAD TO FSMA

SECTION 204(d) COMPLIANCE

By January 20th 2026, all food manufacturers must be fully compliant with Section 204(d) of the FSMA (Food Safety Modernization Act). The final rule is a key component of the FDA’s (Food and Drug Administration’s) New Era of Smarter Food Safety Blueprint. Deploying an effective MES (Manufacturing Execution System) such as Plex, by Rockwell Automation is imperative to ensure compliance, avoid disruption, and optimize operations.

WHAT ARE THE FSMA
SECTION 204(d) REQUIREMENTS:

WHAT MANUFACTURERS
MUST CONSIDER:

Provide information to the FDA within 24 hours of a request, either paper or electronic. An electronic sortable spreadsheet is required during an outbreak, product recall, or public health threat.

Maintain records containing Key Data Elements (KDEs) associated with Critical Tracking Events (CTEs).

Establish full traceability and visibility within the four walls of the manufacturing plant for Food Traceability List (FTL) items including all CTE’s and KDE’s, and one up/one down traceability to suppliers and customers.

End to End Traceability: Support for CTEs (and KDEs) from receiving through any number of production transformation steps all the way to shipping, inventory adjustments and physical count changes.

Provide full disclosure of methods used to ensure full traceability.

Leverage a system that supports real-time tracking of manufacturing processes and lot usage, providing a foundation for FSMA Section 204(d) reporting compliance.

Utilize a centralized system that provides a single source of truth and lot traceability information for all company personnel and auditors.

PLEX SMART MANUFACTURING PLATFORM

LOT TRACKING & TRACEABILITY REPORTING TO ENABLE:

Identification of items on the FTL.
Support for KDEs (and CTEs) through any number of production transformation steps (shipping, receiving, inventory adjustments, and physical count changes).
Mass balance & quantity reconciliation for forward trace of received goods.

Risk Reduction
Product recall support: Reduced risk and cost of recalls via precise containment of suspect inventory and minimization of recall scope.
Centralized, cloud-based system accessible from any location.

Recall Management
Real-time records of all lot traceability events supporting forward and backward trace from origin to destination and vice versa.
Instant access to historical and current traceability data for all FTL goods to support streamlined auditing.
Ability for food manufacturers to demonstrate fast and powerful trace capabilities with full FMSA Section 204(d) compliance to retain existing retail customers and attract new ones.

www.plex.com/industries/food-and-beverage

www.abiresearch.com

www.plex.com

We Empower Technology Innovation and Strategic Implementation. ABI Research is uniquely positioned at the intersection of end-market companies and technology solution providers, serving as the bridge that seamlessly connects these two segments by driving successful technology implementations and delivering strategies that are proven to attract and retain customers. +1.516.624.2500 in the Americas, +44.203.326.0140 in Europe, +65.6592.0290 in Asia-Pacific or visit www.abiresearch.com. ALL RIGHTS RESERVED. No part of this document may be reproduced, recorded, photocopied, entered into a spreadsheet or information storage and/or retrieval system of any kind by any means, electronic, mechanical, or otherwise without the expressed written permission of the publisher. Exceptions: Government data and other data obtained from public sources found in this graphic are not protected by copyright or intellectual property claims. The owners of this data may or may not be so noted where this data appears. Electronic intellectual property licenses are available for site use. Please call ABI Research to find out about a site license. ©2024 ABI Research

Featured Resources

Loading
Loading
Loading